:TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WDISplayed
Command Syntax
:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:PAYLoad:WDISplayed <num_words>
Where N identifies one of four possible protocol decodes {1:4}. For example, SEARch3.
Where F identifies one of three possible fields {1:3}. For example, FIELd2.
Where <num_words> is an integer from 1 to 32.
Query Syntax
:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:PAYLoad:WDISplayed?
Description
This command specifies the number of words in the protocol qualified trigger field.