:TRIGger:QUALify:PROTocol:SEARch:FIELd:RESet

Command Syntax

:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:RESet

Where N identifies one of four possible protocol decodes {1:4}. For example, SEARch3.

Where F identifies one of three possible fields {1:3}. For example, FIELd2.

Description

Resets the protocol qualified trigger options to their default values and resets the defined payload.