:TRIGger:QUALify:ZONE:ZONE{N}:STATe
Command Syntax
:TRIGger:QUALify:ZONE:ZONEN:STATe {ON | OFF | 1 | 0}
Where N identifies one of eight possible zones {1:8}. For example, ZONE2.
Query Syntax
:TRIGger:QUALify:ZONE:ZONEN:STATe?
Query Response
{1 | 0}
Description
Enables or disables the specified zone as part of the zone qualified trigger.
Use the :TRIGger:QUALify:MODE command to select the type of qualified trigger.