:TRIGger:QUALify:MEASure:REGion

Command Syntax

:TRIGger:QUALify:MEASure:REGion  {INSide | OUTSide}

Query Syntax

:TRIGger:QUALify:MEASure:REGion?

Description

For measurement qualified triggers (see :TRIGger:QUALify:MODE) and the selected measurement (see :TRIGger:QUALify:MEASure:LOCation) and its measurement limits (see :TRIGger:QUALify:MEASure:LLIMit and :TRIGger:QUALify:MEASure:ULIMit), this command specifies whether results inside or outside the limits are used to qualify triggers.