:TRIGger:QUALify:PROTocol:SEARch:FIELd:FORMat

Command Syntax

:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:FORMat  {HEX | DECimal | BINary | DCODe}

Where N identifies one of four possible protocol decodes {1:4}. For example, SEARch3.

Where F identifies one of three possible fields {1:3}. For example, FIELd2.

Query Syntax

:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:FORMat?

Description

Depending on the selected protocol (see :TRIGger:QUALify:PROTocol:SELected), this command selects the number format for specifying word values.

Search field formats available for protocol types
Protocol type Display formats
G8B10B {HEX | DECimal | BINary | DCODe}
GRAW {HEX | DECimal | BINary | OCTal}

D Code values are formatted like "Dnn.n", for example, "D28.3".