:TRIGger:QUALify:ZONE:ZONE{N}:LOGic

Command Syntax

:TRIGger:QUALify:ZONE:ZONEN:LOGic  {AND | OR | NAND | NOR}

Where N identifies one of eight possible zones {1:8}. For example, ZONE2.

Query Syntax

:TRIGger:QUALify:ZONE:ZONEN:LOGic?

Description

Selects the type of the specified zone and the logic used to combine other zones used for the same signal:

  "Must Intersect" "Must Not Intersect"
Zones for the same signal are "ANDed" AND NAND
Zones for the same signal are "ORed" OR NOR

Use the :TRIGger:QUALify:ZONE:ZONE{N}:SOURce command to select the signal on which the zone operates.