:TRIGger:QUALify:MEASure:LOCation
Command Syntax
:TRIGger:QUALify:MEASure:LOCation <measurement_source>
Where <measurement_source> is the number of the measurement according to the top-to-bottom order in the Measurement results window.
Query Syntax
:TRIGger:QUALify:MEASure:LOCation?
Description
For measurement qualified triggers (see :TRIGger:QUALify:MODE), this command selects the measurement whose results are used to qualify triggers. Analog input channel measurements or function measurements can be used to qualify triggers.
Measurements on functions are available to be used in measurement qualified triggers except when averaging functions or measurement trend functions are included in the function chain.
Use the :TRIGger:QUALify:MEASure:LLIMit and :TRIGger:QUALify:MEASure:ULIMit commands to specify the lower and upper measurement result limits.
Use the :TRIGger:QUALify:MEASure:REGion command to specify whether results inside or outside the limits are used to qualify triggers.