:TRIGger:QUALify:ZONE:ISZLogic
:TRIGger Qualify Commands
- :TRIGger:QUALify:FOQualify
- :TRIGger:QUALify:MEASure:LLIMit
- :TRIGger:QUALify:MEASure:LOCation
- :TRIGger:QUALify:MEASure:REGion
- :TRIGger:QUALify:MEASure:ULIMit
- :TRIGger:QUALify:MODE
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:ETYPe
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:FORMat
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:FTYPe
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:RESet
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WDISplayed
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WORD:OPERand
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WORD:POPerator
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WORD:RESet
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WORD:SYMBol
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WORD:TYPE
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:WSIZe
- :TRIGger:QUALify:PROTocol:SEARch:FIELd:RESet
- :TRIGger:QUALify:PROTocol:SEARch:GTYPe
- :TRIGger:QUALify:PROTocol:SEARch:PTYPe
- :TRIGger:QUALify:PROTocol:SEARch:RESet
- :TRIGger:QUALify:PROTocol:SEARch:SOURce
- :TRIGger:QUALify:PROTocol:SELected
- :TRIGger:QUALify:PROTocol:SELected:COPY
- :TRIGger:QUALify:STATe
- :TRIGger:QUALify:ZONE:ISZLogic
- :TRIGger:QUALify:ZONE:ZONE{N}:LOGic
- :TRIGger:QUALify:ZONE:ZONE{N}:SOURce
- :TRIGger:QUALify:ZONE:ZONE{N}:STATe
- :TRIGger:QUALify:ZONE:ZONE{N}:X
- :TRIGger:QUALify:ZONE:ZONE{N}:Y
Command Syntax
:TRIGger:QUALify:ZONE:ISZLogic {AND | OR}
Query Syntax
:TRIGger:QUALify:ZONE:ISZLogic?
Description
When zone qualified triggers are enabled (see :TRIGger:QUALify:MODE), this command specifies the Inter Signal Zone Logic, that is, the logic used when combining the zones of different signals.