:TRIGger:QUALify:PROTocol:SEARch:FIELd:PAYLoad:RESet
Command Syntax
:TRIGger:QUALify:PROTocol:SEARchN:FIELdF:PAYLoad:RESet
Where N identifies one of four possible protocol decodes {1:4}. For example, SEARch3.
Where F identifies one of three possible fields {1:3}. For example, FIELd2.
Description
Resets the defined payload to "don't care" values (without resetting other protocol qualified trigger options, as is done with the :TRIGger:QUALify:PROTocol:SEARch:FIELd:RESet command).