:TRIGger:QUALify:MEASure:ULIMit
Command Syntax
:TRIGger:QUALify:MEASure:ULIMit <upper_limit>
<upper_limit> is a double.
Query Syntax
:TRIGger:QUALify:MEASure:ULIMit?
Description
For measurement qualified triggers (see :TRIGger:QUALify:MODE) and the selected measurement (see :TRIGger:QUALify:MEASure:LOCation), this command specifies the upper measurement result limit.
Use the :TRIGger:QUALify:MEASure:LLIMit command to specify the lower measurement result limit.
Use the :TRIGger:QUALify:MEASure:REGion command to specify whether results inside or outside the limits are used to qualify triggers.