:TRIGger:QUALify:PROTocol:SELected

Command Syntax

:TRIGger:QUALify:PROTocol:SELected <protocol_decode>

Where <protocol_decode> can be one of the following:

  • PROTocol{1:4}

Query Syntax

:TRIGger:QUALify:PROTocol:SELected?

Description

Selects the protocol decode used in the protocol qualify trigger.

Use the :TRIGger:QUALify:PROTocol:SELected:COPY command to copy the protocol decode's search setup to its protocol qualified trigger setup. If NONE is returned by the query, the :TRIGger:QUALify:PROTocol:SELected:COPY command does nothing.