:TRIGger:QUALify:MEASure:LLIMit
Command Syntax
:TRIGger:QUALify:MEASure:LLIMit <lower_limit>
<lower_limit> is a double.
Query Syntax
:TRIGger:QUALify:MEASure:LLIMit?
Description
For measurement qualified triggers (see :TRIGger:QUALify:MODE) and the selected measurement (see :TRIGger:QUALify:MEASure:LOCation), this command specifies the lower measurement result limit.
Use the :TRIGger:QUALify:MEASure:ULIMit command to specify the upper measurement result limit.
Use the :TRIGger:QUALify:MEASure:REGion command to specify whether results inside or outside the limits are used to qualify triggers.