Noise Figure on Converters (NFX) - S9x029A/B


This topic discusses Noise Figure on Converters:

The following general information (contained in Noise Figure Application for Amplifiers) is also relevant for NFX measurements:

Other Application Topics

Requirements and Limitations

Noise Figure on Converters requires Noise Figure ( S9x029A/B).

M983xA Option 029: These options activates high gain in Receiver Gain

 

Learn more about Noise Figure requirements.

Limitations

The following VNA features are NOT available with NFX:

Embedded LO measurements ARE supported in NFX. Learn more.

How to Configure your Hardware

DUT Configuration

Learn more about connecting the DUT input and output to the VNA.

The DUT LO can be connected to an external source OR VNA internal second source (if available).

Select an LO Source on the Mixer Setup tab.

Note: Noise that is present on the LO source will be directly transferred to the DUT output. This noise can NOT be calibrated out of the noise measurement. Therefore, choose a low-noise source for the LO, such as an Keysight ESG or PSG, which is better than the VNA internal source.

Using the Noise Figure Application

Use the following general procedure to make measurement with the Noise Figure App:

  1. Connect Tuner and Noise Source.

  2. Create a Noise Figure Measurement.

  3. Make Noise Figure Settings.

  4. When 346 Seis noise source is used, copy your Noise Source ENR file to the VNA C:\Program Files(x86)\Keysight\Network Analyzer\Noise folder.

  5. Perform Calibration

  6. Connect the DUT. Learn more.

  7. Measure Noise Figure.

  8. Optional  Click File, then Save to save Noise Figure data in the following formats: (available ONLY when NF correction is ON.)

See Also: Measurement Tips

Connect Noise Tuner and Noise Source

  1. Connect the noise source .  The Noise Source is turned ON and OFF automatically as needed during a calibration. Connect the noise tuner to Port 2 reference place when prompted during calibration.

  2. Connect the noise tuner (ECal module). NOT required for 50 GHz models and  Scalar Noise Figure measurements.

    1. On the VNA front panel, remove the Port 1 jumper cable SOURCE OUT / CPLR THRU. Opt 028 allows Noise Figure measurements using any two VNA ports. Connect the noise tuner to the front-panel jumpers for the source (DUT input) port.

    2. Connect M-F tuner (N4691B-M0F) using the supplied cable (N5242-20137) and adapter (85052-60013).

    3. When using F-F ECal module (N4691B-00F), order a 3.5 mm M-M adapter (85052-60014).

Create a Noise Figure Measurement

  1. On the VNA front panel, press Meas > S-Param > Meas Class....

  2. Select Noise Figure Converters, then either:

  1. A Noise Figure measurement is displayed. Do the following to add or change parameters to display.

NFX Parameters

How to ADD NFX Parameters

  1. Create an NFX channel.

  2. Then do the following:

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Press Trace > Trace N >  Trace N.

  2. Press Trace > Trace Setup >  Measure....

  1. Click Instrument

  2. Select Trace

  3. Select Add Trace

  4. Click Instrument

  5. Select Trace

  6. Select Measure...

How to CHANGE NFX Parameters

  1. Create an NFX channel.

  2. Select the parameter to change.

  3. Then do the following:

  1. Select a trace by pressing Trace > Trace N >  Trace N.

  2. Press Trace > Trace Setup >  Measure....

  3. Select a parameter.

  1. Right-click on a trace.

  2. Select a parameter

Programming Commands

The same Noise parameters that are available in the Noise Figure application are also available in the NFX application. Learn more.

In addition, the following Mixer and Raw Receiver parameters are available in an NFx channel:

Mixer Parameters

Raw Receiver Parameters

Specify a receiver to measure at LO1 frequencies with the notation:

Specify a receiver to measure using a source port, with the notation:

How to start the Noise Figure Setup dialog

Using Hardkey/SoftTab/Softkey

Using a mouse

  1. Freq > Main >  NFX Setup....

  1. Click Stimulus

  2. Select NFX Setup...

Programming Commands

Valid Mixer Configuration / Sweep Type Combinations

The following are the Valid Mixer Configurations:

Sweep Type

Input

LO

Output

Linear

Swept

Swept

Fixed

Swept

Fixed

Swept

CW

Fixed

Fixed

Fixed

Fixed

Swept

Swept

For determining a valid mixer configuration with 2 LOs, one Fixed LO and one Swept is equivalent to having a single-stage Swept LO.

If you create an invalid Sweep Type / Mixer Configuration, a red message appears like the following:

If this occurs, change the Sweep Type on the Frequency tab.

See other rules for configuring a mixer.

 

The following tabs are available on the NFX Setup dialog:

Frequency tab - NFX Setup dialog box help

Sweep Type

Linear - Use for Swept Input parameters

CW Frequency - Use for Fixed Input parameters

X-Axis Display

Annotation: Select the frequency range to display on the X-axis.

Sweep Settings

Click to learn more about these settings.

Learn about the Load/Save *.mxr files, and other buttons across the bottom of all NFX Setup tabs.

 

Power Tab - NFX Setup dialog box help

Learn about this dialog.

Learn about the Load/Save *.mxr files, and other buttons across the bottom of all NFX Setup tabs.

 

 

NFx Noise Figure Setup dialog box help

This dialog is identical to the Noise Figure Setup for amplifier EXCEPT for the following setting. Learn about the rest of this dialog.

Enable Source Pulling for S-Parameters (For mixers with low reverse isolation). When checked, during S22 (output match) measurements, the noise tuner is switched to present different impedance states to the DUT input. From these measurements, S22 is computed as though the input is seeing a 50 ohm match. This requires more sweeps. Check this box when the converter has low reverse isolation, as is the case when the NO output path is NOT padded with attenuation. Otherwise, clear this checkbox as S22 measurements will not be improved.

An accurate S22 measurement is essential when measuring S-parameters during an NFX calibration.

Learn about the Load/Save *.mxr files, and other buttons across the bottom of all NFX Setup tabs.

 

Mixer Frequency tab - NFX Setup -dialog box help

Learn about this dialog.

 

Mixer (LO) Power tab - NFX Setup dialog box help

Learn about this dialog.

 

Mixer Setup tab - NFX Setup dialog box help

Learn about this dialog.