Last updated: 2010-04-21
The SETup subsystem is used to configure the test set for each measurement. Typical settings include:
Multi-Measurement Count, how many measurements will be made each time a measurement is initiated.
Trigger Arm, determines if a measurement will make one measurement then return to idle (single), or automatically rearm on completion of a measurement and repeat the process (continuous).
Trigger Source, how a measurement is triggered.
Trigger Delay, controls the delay time between the trigger and the start of sampling.
Measurement Timeout, length of time before a measurement times out.