:CALibrate:OPTical:FACTory:CHANnel:STATus:TIME?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:OPTical:FACTory:CHANnel{1:8}{A|B|C|D}:STATus:TIME?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries the date and time when the last N1000A frame calibration was performed. If a calibration has not yet been performed, an empty string is returned.
Requires FlexDCA revision A.02.00 and above.
Example Returned Status String
"08/18/2011 08:14:02"
Example Command
:CALibrate:OPTical:FACTory:CHANnel2B:STATus:TIME?