:CALibrate:OPTical:USER:CHANnel:WSELection
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:OPTical:USER:CHANnel{1:8}{A|B|C|D}:WSELection USER{1:4}
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Query Syntax
:CALibrate:OPTical:USER:CHANnelN:WSELection?
Description
For DCA-M and N1000A plug-in optical modules, selects a user-calibrated wavelength to be deleted using the :CALibrate:OPTical:USER:CHANnel:DISCard command. Up to four user-calibrated wavelength can exist.
Requires FlexDCA revision A.06.00 and above.
Example Command
:CALibrate:OPTical:USER:CHANnel2A:WSELection USER2