:CALibrate:OPTical:CONVersion?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:OPTical:CONVersion CHANnel{N} {USER | WAVelength{1|2|3}}
Where N identifies a specific channel and must be selected from {1:8}{A|B|C|D}. For example, CHANnel3C.
Description
For an optical module, returns the optical conversion (responsivity) of the specified optical channel at the specified wavelength. The arguments WAVelength1, WAVelength2, and WAVelength3 select factory-calibrated wavelengths. If the channel has multiple input connectors (for example, option 004 channels on an 86115D module), the optical conversion reported only applies to the currently selected connector. To query the optical conversion of a different connector, first select that connector with the :CHANnel:CONNector command.
Requires FlexDCA revision A.05.00 and above.
Example Command Sequence
:CALibrate:OPTical:CONVersion? CHANnel2A USER