:CALibrate:OPTical:FACTory:CHANnel:STATus:DETails?
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CALibrate:OPTical:FACTory:CHANnel{1:8}{A|B|C|D}:STATus:DETails?
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Queries a string of status details for the N1000A frame.
Example Returned Status
"15.53 V/W at 850 nm,23.43 V/W at 1310 nm,24.49 V/W at 1550 nm"
Requires FlexDCA revision A.02.00 and above.
Example Command
:CALibrate:OPTical:FACTory:CHANnel2B:STATus:DETails?