:CALibrate:OPTical:USER:CHANnel:DISCard
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:CALibrate:OPTical:USER:CHANnel{1:8}{A|B|C|D}:DISCard
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
Deletes an optical user-calibrated wavelength on the indicated channel. Before you can delete a user-calibrated wavelength, you must select the calibration using the :CALibrate:OPTical:USER:CHANnel:WSELection.
Requires FlexDCA revision A.05.80 and above.
Example Command
:CALibrate:OPTical:USER:CHANnel2A:DISCard