:CALibrate:OPTical:USER:CHANnel:WAVelength
Command Syntax
:CALibrate:OPTical:USER:CHANnel{1:8}{A|B|C|D}:WAVelength <wavelength>
<wavelength> is a double.
Where the required specifier {1:8}{A|B|C|D} identifies a channel by its module slot number and channel letter. For example, channel 3C (CHANnel3C).
The channel specifier will fail if it does not include a slot number. If instead the suffix's channel letter is missing, the command defaults to letter A. As a result, the best practice is to always explicitly specify the channel by including both the module slot number and channel letter.
Description
On DCA-M and N1000A plug-in optical modules, specifies the wavelength at which a user optical calibration is performed. The wavelength of the optical source must be within the allowable calibration requirements. Use the :OPOWer sibling command to specify the wavelenth at which the calibration applies. Use the :STARt command to perform the calibration.
Requires FlexDCA revision A.05.00 and above.
Example Command
:CALibrate:OPTical:USER:CHANnel2A:WAVelength 1.310E-06