:CHANnel CDR Commands (FlexRT)
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Use these :TIMebase subsystem commands to configure how FlexRT applies software clock recovery on all Infiniium channel waveforms. In the GUI, these universal settings are made in the Infiniium Scope Setup dialog. To enable the software clock recovery, use the :TIMebase:SCRecovery:STATe command. By default, software clock recovery is on.
For any selected channel, you can disable or enable these universal (shared) settings so that the channel can have its own unique setting. To do this, use the :CHANnel:RTSCope:TRACk command.