:TIMebase:SCRecovery:STATe
Instrument
N1000A
N109x
Flex Apps:
FlexDCA
Meas. mode:
Scope
Eye
Jitter
Command Syntax
:TIMebase:SCRecovery:STATe {ON | OFF}
Query Syntax
TIMebase:SCRecovery:STATe?
Description
Turns the application of FlexRT software clock recovery ON or OFF. Software clock recovery is applied to the UXR-series oscilloscope's waveforms. The default setting for software clock recovery is on.
This acquisition setting is automatically shared with all UXR oscilloscope input channel waveforms. To independently configure for specific channels, use the :CHANnel:RTSCope:TRACk command.
Requires FlexDCA revision A.06.70 and above.