:CRECovery:CRECovery?
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:CRECoveryN?
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A/B modules, specify slot 1.
Description
Returns the presence of clock recovery hardware. One use of this command is to confirm that an N1092A/B DCA-M extended module has clock recovery hardware installed (Option CDR).
The returned boolean values are:
- 1
- Clock recovery hardware is present.
- 0
- Clock recovery hardware is not present.
Requires FlexDCA revision A.06.50 and above.
This is the only subsystem in FlexDCA where the subsystem's node can be issued as a command or query. In this case, only as a query.