:CRECovery:PRESets:SELections?

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Query Syntax

:CRECovery{1:8}:PRESets:SELections?

Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.

Query Response

"preset name, preset name, preset name, …"

Description

Returns a comma-separated string of all saved clock recovery presets, including factory default presets. Use the :CRECovery:PRESet command to load one of these presets. The following factory presets are included in the returned list:

Clock Recovery Presets

  • CEI-112G-VSR/MR/LR (53 GBd)
  • CEI-25G-LR
  • CEI-28G-SR
  • CEI-28G-VSR/MR
  • CEI-56G-VSR/MR/LR (26 GBd)
  • IEEE 100G-KR4_CR4
  • IEEE 10G-KR_40G-KR4
  • IEEE 40G-CR4_100G-CR10
  • IEEE 802.3bs/cd (26 GBd) NRZ
  • IEEE 802.3bs/cd (26 GBd) PAM4
  • IEEE 802.3bs/cd/ck (53 GBd)
  • IEEE 802.3dj (106 GBd)
  • IEEE 802.3dj (113 GBd)
  • Infiniband EDR
  • PCI Express Gen 3
  • SATA Gen 1
  • SATA Gen 2
  • SATA Gen 3
  • USB 3.0 Gen 1
  • USB 3.0 Gen 2

Requires FlexDCA revision A.04.50 and above.