:CRECovery:PRESets

Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT

Command Syntax

:CRECovery{1:8}:PRESets <preset name>

Where the {1:8} specifier identifies a slot number which is associated with clock recovery module.

<preset name> is a string.

Description

Loads a previously saved or factory provided clock recovery settings known as a preset. The preset configures an N1060A module or N107x-series clock-recovery DCA-M modules with your saved preset settings.

To query which presets are available for loading, use the :CRECovery:PRESet:SELections? query.

Clock Recovery Presets

  • CEI-112G-VSR/MR/LR (53 GBd)
  • CEI-25G-LR
  • CEI-28G-SR
  • CEI-28G-VSR/MR
  • CEI-56G-VSR/MR/LR (26 GBd)
  • IEEE 100G-KR4_CR4
  • IEEE 10G-KR_40G-KR4
  • IEEE 40G-CR4_100G-CR10
  • IEEE 802.3bs/cd (26 GBd) NRZ
  • IEEE 802.3bs/cd (26 GBd) PAM4
  • IEEE 802.3bs/cd/ck (53 GBd)
  • IEEE 802.3dj (106 GBd)
  • IEEE 802.3dj (113 GBd)
  • Infiniband EDR
  • PCI Express Gen 3
  • SATA Gen 1
  • SATA Gen 2
  • SATA Gen 3
  • USB 3.0 Gen 1
  • USB 3.0 Gen 2

Presets can only be saved from the Receiver Setup dialog. There is no programming command for this task.

Requires FlexDCA revision A.04.50 and above.

Example Command Sequence

:CRECovery1:PRESet "PCI Express Gen 3"  //  Load a factory provided preset.
:CRECovery1:PRESet:SELections?  //  Get list of available presets.