:CRECovery:LSELect:AUTomatic
Instrument:
N1000A
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Command Syntax
:CRECovery{1:8}:LSELect:AUTomatic {ON | OFF | 1 | 0}
Where the {1:8} specifier identifies a slot number which is associated with clock recovery module. On 86108A modules, specify slot 1.
Query Syntax
:CRECovery{1:8}:LSELect:AUTomatic?
Query Response
{1 | 0}
Description
Turns on or off automatic selection of the Type-2 loop transition frequency (peaking) module. When turned off, use the :CRECovery:LSELect command to manually select the frequency.
Command Compatibility
- 83496A/B Option 300