:CRECovery:LOCKed?
Instrument:
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
Flex Apps:
FlexDCA
FlexRT
FlexPLL
Query Syntax
:CRECoveryN:LOCKed?
Where N identifies slot number {1:8} which is associated with clock recovery module. On 86108A modules, specify slot 1.
Description
Returns the locked status of the clock recovery module.
For 83496A/B modules, the trigger output to the mainframe is not disabled when an unlocked condition exists.
The returned values are:
- 1
- Clock recovery is locked.
- 0
- Clock recovery is not locked.
Command Compatibility
- N107x-Series DCA-M
- N1092A/B DCA-M Option CDR
- 86108A/B
- 83496A/B