:DISPlay:JITTer:ASPectrum:EDGE
Meas. mode:
Jitter
Package License:
L-RND
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JITTer:ASPectrum:EDGE {FEDGe | REDGe | BEDGes}
Query Syntax
:DISPlay:JITTer:ASPectrum:EDGE?
Description
Sets the edges on which to base Jitter Mode's Aliased Jitter Spectrum graph. To display the graph, use the :DISPlay:JITTer:GRAPH:TYPE command. The default value is REDG.
BEDGes- Because the Aliased Spectrum graph can only be set to use Rising or Falling edges, if
BEDGesis selected, this graph defaults to using Rising edges. FEDGe- Selects the falling edges.
REDGe- Selects the rising edges.
Requires FlexDCA revision A.05.60 and above.