:DISPlay:JITTer:LAYout
Meas. mode:
Jitter
Package License:
L-RND
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JITTer:LAYout {SINGle | SPLit | QUAD}
Query Syntax
:DISPlay:JITTer:LAYout?
Description
Selects the maximum number of Jitter/Noise Mode graphs displayed at one time. The arguments have the following definitions:
- SINGle
- One graph is displayed.
- SPLit
- Two graphs are displayed.
- QUAD
- Four graphs are displayed. This is the default setting.