:DISPlay:JITTer:CCEdge
Meas. mode:
Jitter
Package License:
L-RND
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JITTer:CCEDge
Query Syntax
There is no query form of this command.
Description
Toggles the set of edges shown on Jitter Mode's edge model graph (titled Edge Curve Model. Normally, there is only one set of edges displayed on the graph and this command has no effect. However, if the pattern length is even, the Cycle Edges button is shown on the graph which allows you to toggle the view to another set of edges. This command is equivalent to clicking the Cycle Edges button.
Requires FlexDCA revision A.02.50 and above.