:DISPlay:JSANalysis:SGRaph
Meas. mode:
Scope
Eye
Jitter
Feature:
JSA
Waveforms:
NRZ
PAM4
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JSANalysis:SGRaph {ON | OFF | 1 | 0}
Query Syntax
:DISPlay:JSANalysis:SGRaph?
Query Response
{1 | 0}
Description
Displays (ON) or hides (OFF) the JSA Spectrum graph. The default setting is OFF.
Requires a module with Option JSA. Jitter Spectrum Analysis and SW Clock Recovery Emulation .
Requires FlexDCA revision A.01.70 and above.