:DISPlay:JITTer:EYE
Meas. mode:
Jitter
Package License:
L-RND
Flex Apps:
FlexDCA
Command Syntax
:DISPlay:JITTer:EYE {EYE2 | EYE1 | EYE0}
Query Syntax
:DISPlay:JITTer:EYE?
Description
For PAM4 signals in Jitter Mode, select one of three PAM4 eyes on which to base the displayed jitter graphs. The selected eye is indicated in each graph's label.

Requires FlexDCA revision A.05.60 and above.