:FUNCtion:PATTern:FILE:NAME
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:PATTern:FILE:NAME <file name>
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Where <file name> is the name, including path, to a pattern file.
Query Syntax
:FUNCtion{1:64}:PATTern:FILE:NAME?
Description
Enters the name of a BERT pattern file (*.ptrn) when the :FUNCtion:PATTern:MODE command has been used to turn autodetection of the Pattern Symbol Sequence off and specified that a pattern file be used instead. If the name of the pattern file has already been entered (as returned by the query form of this command), you can use the :FUNCtion:PATTern:FILE:RELoad command instead.
This command can be used with the following Signal Processing functions:
Requires FlexDCA revision A.07.40 or greater.
Example Command
:FUNCtion2:PATTern:FILE:NAME "C:\Documents\Keysight\FlexDCA\Patterns\test-pattern.ptrn"