:FUNCtion:PATTern:TRACking
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:PATTern:TRACking {OFF}
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion{1:64}:PATTern:TRACking?
Description
Turns the tracking of the waveform's Pattern Symbol Sequence on or off. Tracking allows the function to adapt to changes to the signal's pattern.
This command can be used with the following Signal Processing functions:
Requires FlexDCA revision A.07.40 or greater.
Example Command
:FUNCtion2:PATTern:TRACking OFF