:FUNCtion:PATTern:FILE:RELoad
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:PATTern:FILE:RELoad
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Description
Reloads a BERT pattern file (*.ptrn) that has previously been loaded using the :FUNCtion:PATTern:FILE:NAMe command.
This command can be used with the following Signal Processing functions:
Requires FlexDCA revision A.07.40 or greater.
Example Command
:FUNCtion2:PATTern:FILE:RELoad