:FUNCtion:PATTern:FORMat
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
TDR
Package License:
L-RND
Command Syntax
:FUNCtion{1:64}:PATTern:FORMat {NRZ | PAM4}
Where the {1:64} specifier identifies one of sixty four math functions that you can create. For example, :FUNCtion2.
Query Syntax
:FUNCtion{1:64}:FORMat?
Description
Specifies the format of the waveform that is input to the equalizer: NRZ or PAM4. You would use this command whenever you have turned off automatic detection of the waveform's Pattern Symbol Sequence with the :FUNCtion:PATTern:MODE command.
This command can be used with the following Signal Processing functions:
Requires FlexDCA revision A.07.40 or greater.
Example Command
:FUNCtion2:PATTern:FORMat PAM4