:JSAMemory:DSTatus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Query Syntax
:JSAMemory:DSTatus?
Query Response
{CORR | INV}
Description
Returns the status of the Jitter Spectrum Analysis (JSA) memory. To query the reason for the current state of the memory, use the :JSAMemory:DSTatus:REASon? query. The following responses can be returned:
CORR- The JSA memory contains JSA data. To clear memory, use the
:JSAMemory:CLEarcommand. INV- The JSA memory location does not contain JSA data.
Requires FlexDCA revision A.05.70 and above.