:JSAMemory:INTegrate:F
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Command Syntax
:JSAMemory:INTegrate:F{1 | 2}
Returns <frequency> which is a double.
Query Syntax
:JSAMemory:INTegrate:F{1 | 2}?
Description
Sets the upper and lower frequency integration FFT limits for the jitter spectrum. Use F1 to set the lower frequency limit and F2 to set the upper frequency limit. On the displayed Jitter Spectrum graph, the
and
symbols show the location of the integration limits.
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.
Requires FlexDCA revision A.02.50 and above.