:JSAMemory:STATus?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Query Syntax
:JSAMemory:STATus?
Query Response
{AVA | UNAV}
Description
Queries the availability of a JSA memory for use. JSA memory becomes available (AVA) after data has been loaded into memory using the :JSAMemory:FILE:LOAD command. The waveform memory does not need to be displayed to be classed as available. A JSA memory is unavailable (UNAV) if data has not been loaded into the memory.
JSA requires an 86108A/B module with Option JSA. To use JSA in Jitter Mode, L-RND package license (includes feature F-JIT Enhanced Jitter Analysis) is required.
Requires FlexDCA revision A.02.50 and above.