:JSAMemory:DSTatus:REASon?
Instrument:
N1000A
N109x
UXR Scope
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Scope
Eye
Jitter
Waveform type:
NRZ
PAM4
Package License:
L-RND
L-SNT
Query Syntax
:JSAMemory:DSTatus:REASon?
Query Response
<string>
Description
Returns a description of the status of the Jitter Spectrum Analysis (JSA) memory. If an JSA data is currently in the JSA memory, a date string for the data is returned. If the Jitter Data memory is empty, the string "Please select a file." is returned. If the file is corrupt or an incorrect type, the string "Unable to load file." is returned. To check the status of the JSA memory, use the :JSAMemory:DSTatus? parent query.
Requires FlexDCA revision A.05.70 and above.