:MEASure:EYE:OER:SOURce

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8

Command Syntax

:MEASure:EYE:OOMA:SOURce <source_waveform>

Where <source_waveform> can be one of the following:

  • CHANnel{1:8}{A|B|C|D}
  • DIFF{1:4}
  • CGMemory{1:8}
  • FUNCtion{1:16}

Query Syntax

:MEASure:EYE:OER:SOURce?

Description

Selects the source waveform on which to perform the OER measurement.

Requires FlexDCA revision A.05.60 and above.