:MEASure:EYE:OER:STATus?
Query Syntax
:MEASure:EYE:OER:STATus?
Query Response
{CORR | INV | QUES}
- CORR
- The measurement result is correct.
- INV
- The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
- QUES
- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the OER measurement. Use the :STATus:REASon? child query to determine the reason for an invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.
Measurement Identification
Avoid subtle programming errors! To ensure that the correct measurement is installed or queried, always explicitly identify a measurement when installing a measurement or querying a measured value, status, or detail. To identify a measurement, specify the measurement's source waveform (:SOURce child command). With some measurements, you may also need to specify other identifying values. Generally, when selecting a measurement using FlexDCA's GUI, if a dialog appears prompting you to select values, you should explicitly specify these values when remotely identifying the measurement. More information.
For example, to return the status of the measurement, :MEASure:EYE:OER
flex.write(':MEASure:EYE:OER:SOURce CHAN1A')
if flex.query(':MEASure:EYE:OER:STATus?') == 'CORR';
measurement = flex.query(':MEASure:EYE:OER?')
else:
details = flex.query(':MEASure:EYE:OER:STATus:DETails?')
reason = flex.query(':MEASure:EYE:OER:STATus:REASon?')
Requires FlexDCA revision A.05.60 and above.