:MEASure:EYE:OER:UNITs
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
NRZ
PAM4/6/8
Command Syntax
:MEASure:EYE:OER:UNITs {DECibel | PERCent | RATio}
Query Syntax
:MEASure:EYE:OER:UNITs?
Description
Selects the units of measurement for the PAM4 outer extinction ratio measurement (:MEASure:EYE:OER). The measurement unitis can be decibels, percent, or ratio.
Requires FlexDCA revision A.05.60 and above.