:MEASure:EYE:PAM:LEVel:LEVel
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4/6/8
Command Syntax
:MEASure:EYE:PAM:LEVel:LEVel LEVel{0:7}
Query Syntax
:MEASure:EYE:PAM:LEVel:LEVel?
Description
Selects the PAM4/6/8 eye diagram's level on which to perform the :MEASure:EYE:PAM:LEVel measurement. If you experience difficulties measuring a PAM signal, confirm that the signal-type setting is set to PAM4, PAM6, or PAM8 with the :CHANnel:SIGNal:TYPE command.
Requires FlexDCA revision A.04.50 and above.