:MEASure:PAM:OSCilloscope:LRMS:LEVel
Meas. mode:
Scope
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:OSCilloscope:LRMS:LEVel{N} <double>
Where {N} is an integer that represents one of four PAM4 levels.
Where <double> is the RMS amplitude of the specified level.
Query Syntax
:MEASure:PAM:OSCilloscope:LRMS:LEVel{N}?
Description
Enters the RMS values for a PAM4 level into memory for use by FlexDCA. This makes these values available for Eye Mode's PAM features such as eye contours and and Advanced Eye Analysis. To automatically load the RMS level values from Oscillosope Mode's PAM Levels RMS measurement (:MEASure:OSCilloscope:PAM:RMS) into memory use the :MEASure:PAM:OSCilloscope:LRMS:GALL command.
Requires FlexDCA revision A.05.60 and above.