:MEASure:PAM:OSCilloscope:LRMS:GALL
Meas. mode:
Scope
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:OSCilloscope:LRMS:GALL
Description
Loads the RMS values from Oscillosope Mode's PAM Levels RMS measurement into memory for use by FlexDCA. This makes these values available for Eye Mode's PAM features such as eye contours and Advanced Eye Analysis. The Levels RMS measurement must be active before sending this command. The values can be manually entered or queried using the :MEASure:PAM:OSCilloscope:LRMS:LEVel command.
Requires FlexDCA revision A.05.60 and above.