:MEASure:PAM:EYE:TIME:UNITs
Meas. mode:
Eye
Package License:
L-RND
L-MFG
Waveform type:
PAM4
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:MEASure:PAM:EYE:TIME:UNITs {SECond | UINTerval}
Query Syntax
:MEASure:PAM:EYE:TIME:UNITs?
Description
Sets the time units for PAM4 width and skew measurements. The units can be seconds (SECond) or unit interval (UINTerval). The following measurements are affected by this setting:
- Eye/Mask Mode
- PAM Level Skews (
:EYE:PAM:SKEW) - PAM Eye Skews (
:EYE:PAM:ESKew) - PAM Eye Widths (
:EYE:PAM:EWIDth) - Oscilloscope Mode
- No PAM Oscilloscope mode measurements are affected by this command.
Requires FlexDCA revision A.04.50 and above.