:RDCA:CONNect:ACTion
Instrument:
DCA-X
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:RDCA:CONNect:ACTion {DSETtings | TBSettings | RPSettings | ASFSettings}
Description
Selects from one of four possible actions that occur whenever FlexDCA connects to the DCA-X (:RDCA:CONNect
). The query returns the current setting. The following four arguments can be specified:
- RPSettings
- Restores the 86100D settings to the same settings used the last time FlexDCA was connected.
- TBSettings
- Copies the 86100D's front-panel related settings into FlexDCA.
- DSETtings
- Defaults all settings.
- ASFSettings
- Starts the application with settings that have been saved to a setup file (.setx). The 86100D is set to the same settings. By default, setup files are saved to the "
My Documents/Keysight/FlexDCA/Setups
" folder located on the PC. To specify the setup file, use the:RDCA:CONNect:SFILe
command.