:RDCA:CONNect:SFILe
Instrument:
DCA-X
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:RDCA:CONNect:SFILe "filename"
"filename" is a string.
Query Syntax
:RDCA:CONNect:SFILe?
Description
Specifies the FlexDCA setup file used to configure the FlexDCA's settings when connecting to an 86100D. You must also specify that a setup file is used when the connection is estableshed (:RDCA:CONNect:ACTion
command with the ASFSettings
argument). Setup files use the .setx file extension and by default is located in the \Setups folder.