:REPository:CONNect
Command Syntax
:REPository:CONNect
Description
Establishes a connection to the specified N8844A data repository server. Specify the N8844A data repository server's URL with the :REPository:SERVer:NAME
command and the service-account name with the :REPository:MEASure:PUBLish:NAME
command. Use the :STATe?
child query to determine the state of the connection.
You must use the Repository Setup dialog the first time that you make a connection to a specific N8844A server. This is because the dialog allows you to enter the account's password which you cannot do using remote commands.
Use of an *OPC?
query to pause program execution while waiting for this command to execute.
Requires FlexDCA revision A.05.70 and above.
Starting with FlexDCA revision A.06.02, a FlexDCA license is no longer required to use FlexDCA with the N8844A Data Analytics Web Service Software.
Child Commands
Example Command Sequence
:REPository:SERVer:NAME "https://123.456.789.12:5000" :REPository:USER "UserName" :REPository:CONNect *OPC?